Prevent unnecessary machine stops: Signal lamp and sensor integration gateway in the production of cardboard trays

Nov 29, 2022

The current trend is cardboard instead of plastic. Machines from the specialist MATEK from France are helping to make sure that cardboard trays are available quickly and efficiently in industry. The experts for end-of-line machines use sensor solutions from SICK to do this: Intelligent use of the SLT signal lamp, the Dx35 mid range distance sensor and the SIG200 sensor integration gateway increases productivity and supports the machine operator.

MATEK has been specializing in end-of-line machines and industrial equipment trading since 2015.
MATEK has been specializing in end-of-line machines and industrial equipment trading since 2015.
MATEK has been specializing in end-of-line machines and industrial equipment trading since 2015 with a range of services from spare parts supply to installation, troubleshooting, machinery improvement and maintenance. MATEK also provides support in designing specific machine parts, especially in the packaging industry. A few years ago, the company also purchased a machine for volumizing cardboard trays to meet the increasing demand for this type of packaging. This was especially important since the latest European directives require a reduction in plastic packaging.

Optimization of machine productivity through ergonomics

The machine in question is a cardboard tray former: At the front, it takes the pre-cut cardboard flat from the loading container, prepares it for volumization, applies the adhesive and completes forming to produce a fully folded tray. An operator is required to fill the magazine at the front and release the stack at the end. The two stations are four meters apart. When operators are at the end of the machine, they cannot see the filling hopper. If it is empty, then the machine stops and reports an error, which greatly reduces productivity.

A signal lamp warns the operator to avoid unnecessary machine stops
From this side of the machine, the operator cannot see the cardboard filling container.
A signal lamp warns the operator to avoid unnecessary machine stops
From this side of the machine, the operator cannot see the cardboard filling container.

To avoid this problem, Mathieu Hartmann, CEO of MATEK, first considered a distance sensor that would initiate a proper machine stop at a certain threshold distance. The Dx35 mid range distance sensor from SICK was perfect for this job. However, since innovation is a building block of MATEK’s DNA, a conversation with Emmanuel Renaud, Regional Sales Account Manager at SICK France, showed that the application could be improved even more. Why not warn the operator with a signal lamp and even a sound to avoid unnecessary machine stops?

The Dx35 mid range distance sensor from SICK initiates a proper machine stop at a certain threshold distance
The Dx35 mid range distance sensor from SICK initiates a proper machine stop at a certain threshold distance

Setup in only three minutes

This is how the SLT signal lamp became part of the project. The 21 colored LEDs now allow a single device to transmit many different types of information and warn the operator at different thresholds. The signal lamp is also equipped with IO-Link, as is the Dx35 mid range distance sensor. That is why Emmanuel Renaud suggested connecting the sensors to a SIG200 sensor integration gateway for easy configuration. And you can really see the result: It only takes three minutes to set up the sensor. “The detection, the blind zones, all the parameters of the sensors connected to the gateway are accessible. It’s amazing how easy it is,” says Mathieu Hartmann from MATEK. After connecting the signal lamp, it took another ten minutes to parameterize the color variations of the column.

Mid range distance sensors
Sensor Integration Gateway
Sensor Visualization
The SIG200 Sensor Integration Gateway can be used to connect signal lamps and the Dx35 mid-range distance sensor.
The SIG200 sensor integration gateway facilitates sensor configuration.
The SIG200 Sensor Integration Gateway can be used to connect signal lamps and the Dx35 mid-range distance sensor.
The SIG200 sensor integration gateway facilitates sensor configuration.

How exactly does it work?

The Dx35 mid range distance sensor is mounted at the top and detects the stack of cardboard in the loading tray at the front of the machine. The SLT signal lamp then reports information about the height of the stack back to the operator:

  • Flashing blue: The magazine is full/more than full
  • Lights up green: The magazine is at 100%
  • Gradual change of the colored section towards yellow between 100% and 50% 
  • Yellow: The magazine is at 50%
  • Gradual change of the colored section towards red between 50% and 20%
  • Addition of an acoustic signal (with the SLB Smart Light Buzzer module) to the red color: Between 20% and 18%
  • Faster and faster flashing between 18% and 1%
  • Below 1%, the machine stops picking up cardboard, but does not stop (no unnecessary restart of the machine)
  • When this level is reached, filling the magazine and pressing a button is enough to restart the machine.

Of course, the goal is never to reach 1% so that productivity is not endangered.

Increase in machine productivity by 5 percent

The subtlety of the machine parameterization is possible thanks to the performance of the SIG200. Since the controller is also connected to the sensor integration gateway, the conditions for stopping the machine can also be set. “The result exceeded my expectations”, explains Mathieu Hartmann. This holistic solution has secured the production cycle, and Hartmann estimates that machine productivity has increased by 5%. The operator can better control the filling process and easily look ahead to what needs to be done. Comfort and ergonomics are motivating factors for an operator. Since the operator actively participated in the parameterization of the colors, confidence in the machine is 100%.

The SLT signal lamp reports information about the height of the stack back to the operator.
Thanks to the SLT signal lamp, the operator knows when to refill the container.
The SLT signal lamp reports information about the height of the stack back to the operator.
Thanks to the SLT signal lamp, the operator knows when to refill the container.

Great sense of trust

The key to the success of this project was above all the great sense of trust between Mathieu Hartmann and Emmanuel Renaud. This trust allowed for open exchange and mutual understanding of the respective requirements. The simplicity and performance of SICK solutions during the demonstration did the rest.

 

Read more

New sensor technology is helping to solve long standing labeling issues

Read more

Every movement in sight: The camera-monitored assembly facility at RIBE Anlagentechnik

Read more