Contact
Feedback

SICK LAUNCHES BRAND NEW TECHNOLOGY FOR ANONYMOUS AND REAL-TIME PEOPLE COUNTING WITH LIDAR

Sep 30, 2020

Accurately monitor occupancy levels in any facility with PeopleCounter SensorApp

 

 
MINNEAPOLIS, MINN., SEPTEMBER 2, 2020 – In reaction to new developments to slow the spread of the COVID-19 virus, SICK has launched its new PeopleCounter (PeCo) SensorApp. Using 3D LiDAR sensors, people can easily maintain recommended occupancy levels in public spaces and in manufacturing settings.
Unlike the use of camera technology, the PeCo LiDAR sensor solution does not process personal information. This ensures companies can maintain any health and safety recommendations, but also that private individuals’ data privacy concerns are being respected. Operators of institutions of public life as well as those that deal in tourism, cruise ships, restaurants, retail, and various other industries can profit from a simple solution that makes it easy to safely maximize utilization of space and still maintain the required occupancy levels.
 
The PeopleCounter (PeCo) is a SensorApp developed by SICK that enables anonymous data processing and differentiation of people from objects over large detection areas. Based on the hardware of the MRS1000 3D LiDAR sensor, measurement data is generated as a point cloud. The integrated PeopleCounter app reliably identifies people using their contours. This means only people above the height of 1.4 meters are counted, while objects are blanked out.
 
Thanks to the four layers of the sensor, the direction of movement of a person is clearly established and the current utilization of a defined zone can be monitored. The recorded data is output digitally to keep track of the maximum number of people allowed in a space. The combination of several sensors makes it possible to cover even large areas with different entry and exit areas, such as shopping centers, airports, or trade shows.
Contact a SICK representative at info@sick.com for more information.
 

 

About SICK

SICK is one of the world’s leading manufacturers of sensors, safety systems, machine vision, encoders and automatic identification products for industrial applications. With more than 1000 patents, SICK continues to lead the industry in new product innovations. The diversity of its product line allows SICK to offer solutions at every phase of production in the logistics, automotive, packaging, electronics, food and beverage, and material handling markets. SICK AG was founded in 1946 and has operations or representation in 65 countries worldwide.

www.sick.com

Contact

Mandee Nguyen
SICK, Inc.
6900 W 110th St
Minneapolis, MN
55438 USA
Phone: 800.325.7425
Fax: 952.941.9287
Email: mandee.nguyen@sick.com

TOP